Hi,
We are trying to develop a board that uses DRV8332. The card is intended to drive four actuators using three phase BLDC motors with maximum Stall torque of 10A.
I have a couple of questions.
1. Is it fine if we connect the RESET-A, RESET-B, RESET-C, pins of the IC to the GPIO's of a DSP processor or Should we connect these pins also to the PWM low pins of the processor.
2. Does DRV8332-HT also support a maximum peak current of 10Amps.
Regards,
Roshan tej.