I would like to use a full H-bridge controller to drive four ST STH310N10F7 N-channel MOSFETs for a 48V load at 25A, at a relatively low frequency (< 1 KHz).
A part like the TI DRV8701E seems like a step in the right direction but the maximum gate drive current (source 150mA / sink 300mA) is still far below what is needed, and it is rated up to 45V rather than 48V.
Are there any TI parts that would be a better fit, or could there be a way to adapt existing parts to fit these requirements?