This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV2511-Q1: Clarification on Datasheet-2

Part Number: DRV2511-Q1

Hello everyone,

I´d like to ask experts to provide extra information about this part.

1. Is there derating curve of peak current with time? I'm interesting in 30ms peak.

2. Is it the recommened part for new developing? It's a litte bit strange that datasheet was not update even it consists wrong description from DRV2510 like NRST pin.

3. I undestand correctly that this part doesn't provide feedback and speed of motor is controled by pre-calculated PWM. So,  for speed control, R sense should be used in serial with motor or to GND.

4. From previous question towards DRV2511 it was said that Rds on is 120mOhm at high temperature (60mOhm at 25). Is it resistance of one Mosfet, p- or n-channel, whatever?

Thanks in advance.

Sobolev