Other Parts Discussed in Thread: , TMS320F28069M, MOTORWARE
Respected sir,
I have interfaced BOOSTXL-DRV8301 REVB to the TMS320F28069M launchpad. I have generated the PWM pulses to drive the gates. In my actual application I just want to drive the single phase bridge so I have generated PWM1A and PWM1B using TMS320f28069M. Now I have to drive the single phase bridge using DRV8301. I don't want to run any motor, I just want to generate the 230V at the output of DRV8301. I don't want the three phase output. What should I do ?
Also there are many lab projects given in MotorWare for InstaSPIN motion using F28069M and DRV8301. Out of them which lab should I use. My purpose is to drive only the single phase inverter bridge of BOOSTXL-DRV8301. I stuck here, so kindly request you to help me out.
Thanks & Regards
Nisha