Other Parts Discussed in Thread: DRV2624EVM-CT
The spec sheet for the DRV2625 states a maximum load impedance of 100pF. WHat happens if the impedance exceeds this value?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
The spec sheet for the DRV2625 states a maximum load impedance of 100pF. WHat happens if the impedance exceeds this value?
Thanks for the response. I cannot find the capacitance listed for LRA's in manufacturers data. Can I use a meter like the Agilent U1731C to measure the capacitance of the motor coil? I used this meter to measure the LRA on a DRV2624EVM-CT board and got the following results:
Resistance = 32 Ohms
Inductance = 192 uH
Capacitance = 132 uF
I cannot find a spec sheet for the ELV1036A Actuator. Is there a better method to determine the capacitance of an LRA?