This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8301: Scalar (V/f) Control of 3-Phase Induction Motor

Part Number: DRV8301
Other Parts Discussed in Thread: MOTORWARE,

Dear All,

I am working on Low voltage Ac induction motor with F28027 and DRV8301 where can i find open loop control example for this, is it avilable in motorware, and where i need to connect wires from motor (red,white,blue) to DRV8301 (A,B,C) do i need to connect 24 V of AC supply to PVDD on DRV8301 

Regards,

Hussain