This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8885EVM: GUIComposerApp behind a Proxy

Part Number: DRV8885EVM


Hallo,

I have some problems while the installing "GUIComposerApp-v1.0.setup-win_2.0.3.exe" behind a proxy.

With the runtime "gcruntime-6.1.0-windows-installer.exe" I get some errors.

gcruntime_6.1.0.20180815074426.log

"Executing C:\Users\honold/guicomposer/runtime/gcruntime.v6/win32/TICloudAgentHostApp/drivers/EZ430UART_64.bat
Script exit code: 256

Script output:
 
C:\Users\honold\guicomposer\runtime\gcruntime.v6\win32\TICloudAgentHostApp\drivers>dpinst_64_eng.exe /path EZ430UART /SW /SA

Script stderr:
 Program ended with an error exit code

Error running C:\Users\honold/guicomposer/runtime/gcruntime.v6/win32/TICloudAgentHostApp/drivers/EZ430UART_64.bat : Program ended with an error exit code
Executing C:\Users\honold/guicomposer/runtime/gcruntime.v6/win32/TICloudAgentHostApp/drivers/xds110_drivers_64.bat
Script exit code: 1280

Script output:
 
C:\Users\honold\guicomposer\runtime\gcruntime.v6\win32\TICloudAgentHostApp\drivers>dpinst_64_eng.exe /path xds110_drivers /SW /SA

Script stderr:
 Program ended with an error exit code

Error running C:\Users\honold/guicomposer/runtime/gcruntime.v6/win32/TICloudAgentHostApp/drivers/xds110_drivers_64.bat : Program ended with an error exit code
Executing C:\Users\honold/guicomposer/runtime/gcruntime.v6/win32/TICloudAgentHostApp/drivers/USB_CDC_64.bat
Script exit code: 256

Script output:
 
C:\Users\honold\guicomposer\runtime\gcruntime.v6\win32\TICloudAgentHostApp\drivers>dpinst_64_eng.exe /SW /SA /path USB_CDC

Script stderr:
 Program ended with an error exit code

Error running C:\Users\honold/guicomposer/runtime/gcruntime.v6/win32/TICloudAgentHostApp/drivers/USB_CDC_64.bat : Program ended with an error exit code
"

Can you please provide me the link to the correct runtime? Or what can I do to start the DRV8885EVM?

Thank you for your help.

Moritz