This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV11873: Sometimes can not spin up a BLDC

Part Number: DRV11873


DRV11873 can not start and spin up the BLDC in small chances, only removing and reconnect the power can fix this.

When this issue happens, RD, FG pin is pulled high, CPN pin is pulled low, U V W COM pins are in DC voltage.

RD pulled low should be indicating a lock protection? What causes this situation?

When motor is running as expected, FG output frequency is 150Hz.

Original link:e2echina.ti.com/.../158369