We have designed a 4-layer PC board with (5) DRV2667 devices on it. We closely followed the recommended PCB layout from the datasheet, but overlooked one feature-- we did not ground or provide thermal vias on the thermal pad. Pins 4-6 are grounded to a copper area.
In addition we inadvertently used a 50V rated capacitor on the BST output (which is programmed for 100V).
Several devices have failed when the boost converter is switched on even with no piezo connected. After the failure the parts exhibit a low (10's of ohms) resistance from BST pin to GND and the part draws excessive current.
Is the GND connection on the pad mandatory for correct no-load operation of the part? Or is it only required when driving a load to cool the device? We do plan to revise the PCB layout but I would like to be confident this is causing the failure. Obviously we will also replace the under-rated capacitor.
Any insight into the type of over-stresses which can cause a catastrophic failure of this part would be helpful.
Thanks!