This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV2605L: can we use the GUI to connect DRV2605L Device

Part Number: DRV2605L
Other Parts Discussed in Thread: USB2ANY,

hello

I got a USB2Any Adapter,  and i connect the DRV2605L with USB2Any Adapter through I2C channel (SCL,SDA, GND).

then connect the other end of USB2ANY with Notebook through USB cable.

I open Haptics control console,  and it can not connect the DRV2605L.

while I can connect the GUI with DRV2605LEVM-CT through USB2ANY. 

So, what should i do if I want use GUI to set or control the DRV2605L device which is mounted on our PCBA board??