Part Number: DRV595
Other Parts Discussed in Thread: DRV2511-Q1,
Hi, what are the differences between DRV595 and DRV2511-Q1 which is 10x cheaper? are the two parts compatible?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: DRV595
Other Parts Discussed in Thread: DRV2511-Q1,
Hi, what are the differences between DRV595 and DRV2511-Q1 which is 10x cheaper? are the two parts compatible?
Hi Andres,
May I know more info about this application? Comparing to DRV595, DRV2411-Q1 can be used for automotive and support as high as 8A output current.
Best regards,
Shawn Zheng
Dear Shawn
Thank you for your reply.
We want to drive peltier elements. As input voltage we are fixed to 24V. I was hoping, that we could use the DRV2511-Q1 with a L-C filter at the output, the same way the DRV595 is implemented in the evaluation boad DRV595EVM.
But the DRV2511-Q1 gives a repeated error at startup in the exact same electronic layout as for the DRV595. Do you have any ideas? From the datasheet, i think it should work. I like the DRV595 but it is to weak for our applications.
Best regards,
Andres