This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8302: query regarding the nOCTW and nFAULT Pin

Part Number: DRV8302

Hi, 

Below is a query from customer regarding the nOCTW and nFAULT Pin.

IN their circuit, The M_OC pin is connected to ground, i.e DRV is in Current limit Mode. When an Over current event occurs, the nOCTW pin goes low, but after that the event nFAULT pin also goes low.

As per the datasheet when DRV is in Current limit mode the OCP event is reported by nOCTW pin and nFAULT pin remains high, but in this case it goes low for 760uS Irregularly.

Can you please suggest the possible reason.