This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8301: DRV8301

Part Number: DRV8301
Other Parts Discussed in Thread: MOTORWARE

Dear All,

I am working on Low Voltage AC Induction Motor with DRV8301 and F28027F and using Motorware lab 2b to run motor. Is their any color coding of leads to leads from motor to be connected to DRV8301 what is range of voltages and Current need to be provided to DRV8301 

  • For motors without an encoder, you can connect the U, V, W phases in any configuration. For the DRV8301, these are the specs:

    6-V to 60-V Operating Supply Voltage Range
    1.7-A Source and 2.3-A Sink Gate Drive Current Capability

    Sean