This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8870: upgrading to higher power device

Part Number: DRV8870
Other Parts Discussed in Thread: DRV8842,

Hi,

I originally did a design to control a 1A brushed dc motor with PWM using the DRV8870 chip.  I was happy with this design, but at the last minute the specification has changed to a 4A brushed dc motor.  Now the DRV8870 is not rated to run a 4A motor, so I need to upgrade.  Would you say the DRV8842 is the best upgrade option to run the 4A motor?

Thanks,

Rocketman46