Part Number: DRV8870
We use the DRV8870 as motor driver at 24V 15kHz to drive a DC 24V motor. Vref = 5V ISEN = GND , VM is connected trough a LC 15µH and 220uF to 24V
For some reason the driver blow up when we block the motor.
The firmware has a stall detection and put the motor in break (both Motor pins at 0V) after 1 second stalling.
Even while the chip have an aditional current and termal protection the chip blow up every time we stall the motor.
What can cause a failure of internal protection circuits in this chip? We already lowered input protection resitors to 10 Ohm.
Thank you