Hello,
I want to buy DRV8704EVM to control DC motor 24V, 30A with Peak Motor Current 80A.
Have you tested the board with the motor with working current like that?
I read spec of Mofet in the DRV8704EVM and it can work.
But the DRV8704EVM doesn't have heatsink or some thing like that, does it can work with 24V 80A without heatsink? If not which heatsink you recommend in this case?
Thanks