I am trying to drive a tiny motor from Nidec called the 17S220F060 at a constant speed of 1000 rpm ( no reverse, it just needs to spin)
No matter what register settings I set, I cannot maintain the motors motion, it keeps stalling. other settings made motor very hot.
the specs are 3 phase, 12 pole & 9 slot
rated voltage 12V
rated current 0.3A
rated speed 11500rpm
coil resistance 3.06 ohm phase to phase
coil inductance 0.36mH
there is no Kt spec.
Can anyone help me select the correct register settings for this motor.