Other Parts Discussed in Thread: DRV8305, , MOTORWARE
Tool/software: Code Composer Studio
Hey.
It is necessary update from DRV8305 to DRV8323. I want to give up SPI management.
I want to buy www.ti.com/.../BOOSTXL-DRV8323RH and work with InstaSpin.
But, in the examples www.ti.com/.../slvc705 there is no code for the Hardware Interface.
The MODE signal has no configuration resistances. :( and stay in HI-Z. - 1xPVM mode.
Forgot set R23 to 0R or to DVDD?
for GAIN R22 must not be. now set 10V/V
I think in the next version this will be fixed.
Andrew.