This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV2605: Auto calibration only required for the closed loop mode

Part Number: DRV2605

Is the auto calibration process only required for the closed loop mode? We are using the drv2605 in the ERM open loop mode.

  • Hi Kanuu,

    Welcome to e2e.
    That's correct, the auto-level calibration can only run on closed loop mode as it needs the back-EMF feedback.
    If using the device in open loop mode the calibration cannot be run so it is not needed.

    Best regards,
    -Ivan Salazar
    Applications Engineer - Low Power Audio & Actuators