Other Parts Discussed in Thread: TMS320F28027F, TMS320F28027
Tool/software: Code Composer Studio
Hello,
I would like to ask about start to drive process on InstaSpin.
I'm using InstaSpin lab5b on TMS320F28027F and DRV8303 on our custom board.
When start to drive motor, for example, changing the value of "refspd" from 0 to 1k,(flag RunIdentify is already set to "1")
sometimes the fault of the Drv8303 occures.
(At first , the motor rotates to reverse direction very slowly,and then Drv8303 fault occures.)
Once could start to drive the motor, there is no problem.
The motor has 7 pole pairs.
I would like to know how to resolve this problem, for example , changing some parameter on user.h or etc.
I would appriciate if someone could reply to my question.
Hiroyasu