This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8806: Do TI has A motor driver chip with HIGH temp down-hole temperature rating?

Part Number: DRV8806


Hi 

I need a high temperature range a driver like the DRV8806 with some clamping voltage pins or simply same function but in operating range (TA) 175°C

Regards