Hello, I'm considering using DRV8833 in a design I am working on. I notice the datasheet is dated from 2011, and the device I'm designing is likely to be in production for a long time, so I was wondering how long TI will continue making DRV8833 for?
I am using it with the H-bridges tied together to drive a brushed DC motor. I specifically require low on-resistance, at least 2A current capability, ability to connect a current sense/limit resistor and ability to run down to 3.3V supply voltage, which this device provides.
If this device is unlikely to be in production for more than a decade, are there plans to replace it with a footprint-compatible equivalent?
Thanks, Tom.