Hi all
Would you mind if we ask DRV8308?
In case of VM=0V, SDATA, FGOUT, FAULTn, LOCK and Reset are connect to VCC=3.3V with pull up resistor as follows;
<Pull-up resistor>
SDATA : 33K
FGOUT : 33K
FAULTn : 33k
LOCK : 33K
RESET : 2.2K
Absolute maximum ratings of SDATA, FGOUT, FAULTn, LOCK and Reset are -0,5V to 5.75V.
Therefore, it is no problem, right?
Just in case, their pins don't have diodes to Vcc, right?
Kind regards,
Hirotaka Matsumoto