This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8886AT: DRV8886AT can connector to Marvell MCU 88DE3006 .

Part Number: DRV8886AT

Hi 

          I need to check:

   1.TI DRV8886AT can connector to Marvell MCU 88DE3006 ?

           2.what is the STEP/DIR control method?

           

                         Thanks

                             JC  Huang

  • Hi JC,

    1) The DRV8886AT can connect to any mcu if:
    a) The GPIO Voh voltage is >1.6V and the GPIO Vol voltage is <0.8V
    b) A PWM output is available to control the STEP pin
    c) A GPIO output is available to control the DIR pin

    2) The STEP/DIR control method uses an internal indexer table to control the stepper motor. Please refer to section 7.3.3 (Microstepping Indexer) of the datasheet for details. The indexer changes the percentage of current according to the table.
  • Hi Duncan

    Thanks you reply.

    JC Huang