This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV10975: DRV10975

Part Number: DRV10975
Other Parts Discussed in Thread: DRV10983

DRV10975 can't spin the motor when the temperature is below -18℃,and the motor can work normally when the temperature is above -18℃

The register settings is as below

DRV10983 0x20 0x7A
DRV10983 0x21 0x3A
DRV10983 0x22 0x2A
DRV10983 0x23 0x8
DRV10983 0x24 0x98
DRV10983 0x25 0xDB
DRV10983 0x26 0x8A
DRV10983 0x27 0xFC
DRV10983 0x28 0xAB
DRV10983 0x29 0xD8
DRV10983 0x2A 0xD
DRV10983 0x2B 0xC

Would you help give any advice