This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8850: LDO is not used

Guru 16770 points
Part Number: DRV8850


Hi

1.

LDO function of DRV8850 is not used in the application.

Could you please tell us adequate termination of LDOEN, LDOFB and LDOOUT?

To saving power, could they be left open?

2.

We will need only forward driving.

Is the following connection correct?

IN1H : PWM

IN1L : ~PWM

IN2H : GND (with 1Kohm)

IN2L : VCC_3.3V (with 1Kohm)

3.

Can we use SR resistor by 2.4Kohm? 

BestRegards