This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV10964: Will it work?

Part Number: DRV10964


We are trying to spin a small BLDC motor with the DRV10964, and it is not running properly (starting and stopping, won't stay running).  I just received some motor parameters (Rm = 2.3 Ohms and Lm = 25 to 30uH) and these are outside of the recommended motor parameters for use with this driver.  Any recommendations for how to get this driver to work?  Or should we give up on the DRV10964?  Any suggestions for a driver that would work for sensorless control of them motor?  This is a 5V bus application.  Thx, Andy