Hi all
Would you mind if we ask DRV8885?
<Question1>
On the datasheet "6.5 Electrical Characteristics", there is QUAD-LEVEL INPUT (DECAY).
According to Decay's resistor, the value of Io(output current) varies.
Is our recognition correct?
<Question2>
On the datasheet Table 6. Decay Mode Settings, there is the description that 45kohm is used for "Mixed decay: 60% fast".
Our customer would like to use 47kohm.
In this case of 47kohm, is the device possible to recognize "Mixed decay: 60% fast"?
There is no 45kohm in case of E48 series, so our customer would like to use E48 series resistor.
Kind regards,
Hirotaka Matsumoto