Part Number: DRV8303EVM
Other Parts Discussed in Thread: INSTASPIN-BLDC
I use the DRV8303EVM board to control the brushless DC motor T-motor air gear 2213/920 kV. The measured maximum speed for this motor is around 11,500 rpm, however I could not reach this speed using DRV8303EVM. I am using InstaSPIN-BLDC_GUI_DRV83xx_v104 software in the velocity control mode. The parameters I set are: 0.01 for flux threshold, Kp = 10, Ki = 0.5, no. of poles =4 and freq. = 500 Hz.
Is there a maximum speed or what is your advice?
Thanks