Hello Team,
What is the maximum Gate Charge DRV8305-Q1 can handle at which frequency?
Thanks.
Best Regards
Joern
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello Team,
What is the maximum Gate Charge DRV8305-Q1 can handle at which frequency?
Thanks.
Best Regards
Joern
Hi Joern - average gate drive current is 30mA. To calculate FET capability use the relationship
Avg Gate drive current = Qg x Freq x (number of FET's switched per cycle)
For trap/block control , number of FET's switched per cycle : 2 or 3
For Since/FOC , number of FET's switched per cycle : 6