Other Parts Discussed in Thread: DRV8711, TIDA-00872
Hi,
my customer need 24V, 3A unipolar stepper motor driver.
Since DRV8805 can only support 2A with single channel on. And 1A per channel when four channel on.
So I think I can use 2 DRV8805 in parallel to achieve 3A current rating.
There are two options:
1. use 2 channels within one drv8805 in parallel, but the datasheet doesn't tell me how much current it can handle when 2 channels are on.
2. Use channel 1 of two drv8805 in parallel, now it should be able to handle totally up to 4A, but I'm not sure if it's okay to use 2 drv8805 in parallel in such way.