Hi Team
Could you help check this qusetion ?
1. The DRV8823 sets its constant current upper limit value by ISEN resistor.
When the ISEN resistor is open or short-circuited at both ends, is the DRV8823 OCP function working on 1.5A~4.5A or OCP function will be disable ?
2. The range of OCP 1.5 to 4.5A is wide. Is there any way to limit it? Does it refer to the OCP protection threshold in the full temperature range?
Thank you so much!!.