This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello All,
Greetings !!!
I am currently working on one project in which we are using DRV8834 motor driver IC and Portescap stepper motor(having 15 degree angle, 400 PPS and 3.6 Volt). The problem that we are facing is related to missing steps when Motor is running in forward and backward direction. We are using Indexer mode configuration. I am describing the problem in detail.
1) Configured DRV8834 to Full step (M0 and M1 are configured to Low Level). but the problem is same, missing the steps of stepper motor.
2) Configured DRV8834 to Half step (M0 is configured to High Level and M1 is configured to Low Level). but the problem is same, missing the steps of stepper motor.
I checked stepper motor steps in debug window but it shows the same steps value every time but still I am getting missed steps. In code I put 2 ms delay also after wake-up from sleep. I have attached schematic screenshot of DRV8834 driver IC.
Please help me to resolve this problem as I am stuck in this since many days.
Thanks,
Nipam
Nipam,
If the winding current doesn't reach the regulation point, that could cause the missing step.
Example: If xVREF is 2 V (as it would be if xVREF is connected directly to VREFO) and a 100-mΩ sense resistor is used, the chopping current will be 2 V / 5 × 100 mΩ = 4 A.
What is the full winding current do you want? Could you measure the winding current to find out which step is missing?
Also, the decay mode setting can affect the winding current waveform. The current setup is 50% OF PWM CYCLE IS FAST DECAY. After we have winding current waveform, we may be able to adjust the decay mode to get a better result.
Dear Wang,
Sure, I resolved this problem 2 days before. The problem is in code in putting DRV8834 in sleep mode. Currently I am not facing any problem with missing steps. I will inform you if any problem will come.
Thanks for your responses on the same.
Thanks,
Nipam