Hi Team,
Could you please recommend several drivers for three-phase current PWM rectifier ?
My Switch Type:MOS ( SPW47N60CFD ) or ( IPW60R045CP )
Driver supply voltage: 12-15V
Thank you !
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello Jiannan,
For this application, single or dual channel isolated approaches will work.
TI created a 3-level, 3-phase AC/DC reference design that uses single channel isolated gate drivers(UCC5320 and ISO5852S) as shown here: 
it can be also be used with dual-channel isolated gate drivers with sufficient spacing between the high-side and the low-side such as the UCC21530 in the DWK (3.3mm spacing) package.
I would like to know why you are choosing MOSFETs for this application? Typically, IGBTs and SiC MOSFETs are used with higher bus voltages and higher gate drives.
If this answered your question, please press the green resolved button.
Regards,
Mateo