This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8323: Current sense amplifier outputs shift one side

Part Number: DRV8323


Hi expert,

After we peformed the auto offset calibration procedure, we are observing an one side offest shift for all current sense outputs (Sox) with +0.07V.

 SOA=SOB=1.64V -> 1.71V

 SOC=1.67 -> 1.74V

Confirmed that Vref is keeping same before/after auto offset calibration.  Do you think this woud happen as a case?

Appreciate any assumption.

Thank you and best regards,

Daisuke KAWASAKI