Tool/software: Code Composer Studio
However, the USB-EMU board has no terminal outputs for GPIO-39/51 as indicated on the DRV830x-HC-C2-KIT_v105 schematics which is needed for the EN_GATE pin. This means I have to use a different spare GPIO, and find in the code where to change it. Or... hardwire it and use the SPI interface to perform RESET_DRV8301. Any suggestions?