Hi
We are using LM48580 and need to measure the quiescent power supply, but it is higher than expected, in LM48580 datasheet, the typical quiescent power consumption at 3.6V should be 2.7mA and maximum is 4mA. But we measured at 3.6V is about 6.3mA (a few boards have similar value), one difference is that we are using 30dB gain(pin 7 is pulled up to Vin), can you provide a typical power consumption under that condition? Thanks.