This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Full-bridge fet driver for IRFP450



Hello

Im driving motor with IRFP450 fets N - CHANNEL - VDGR 500V - 0.33Ω - 14A - VGS 10V

pdf1.alldatasheet.com/.../IRFP450.html

Is there any full bridge drivers from TI what might work with these fets?

Its low rpm motor so no need extremely fast drivers.