Other Parts Discussed in Thread: USB2ANY, DRV11873
hi
I want to control a pump with drv10975. i want to use DRV10975 Evaluation Module.
BUT there are some problems. i study the related documents but i don't know the "USB2ANY" should be connected all of times that motor is driving
or we can separate it after loading and control with potentiometer ?? i mean after we load the parameters we can use the controller without "USB2ANY" or not??
also i don't know if i want to use DRV11873 Evaluation Module how i can change motor poles or it is not needed and how i can add on/off button???
thanks for replying