Hi, team,
My customer has problem for the speed of SPI. Datasheet explains tCLK (Min period) is 100ns(=10MHz) and Rpu is 50kOhms.
He use 1kohms for Rpu but cannot realize the >20MHz SPI.
He use 20 DRV8350 on the SPI line. It may have capacitance.
Do you have idea why they cannot realize 10MHz? and Is there advice for this situation (e.g user should use ???k ohms to realize 100MHz SPI)
Regards,
Nagata.