Hello,
we are using DRV8833 motor driver to drive 3V DC gearmotor with typical current consumption of about 50mA. We would like to know if we must separate 3V power supply applied to VM pin of DRV8833 driver from other electronic parts as RF Bluetooth module, microcontroller, etc. that in this moment are powered with same 3V voltage. I know that when motor is running it put some noise on the 3V power supply line connected to VM pin by means of DRV8833 driver, is it sufficient put large ceramic capacitor (10uF typical) near VM pin of DRV8833 driver to mitigate this phenomena or is it better to use other electronic components (such as, LDO, DC/DC or some filters) interposed from 3V power supply and VM pin?
Many thanks in advance
Francesco