This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8353: Footprint of DRV8353

Part Number: DRV8353

Dear Officials,

I'm testing my motor driver board using the drv8353. Unfortunately, there was a short circuit when power was applied to the board.

During a debugging, I observed that the position of the exposed pad which was showed on page 86 ~ 87 of data sheet is different from the actual chip.

when I cutting the pad a bit with the knife and soldering the chip, there is no short circuit

Please confirm that the exposed pad position of the footprint in the data sheet is correct or incorrect.

Sincerely,

Eui-heon