Other Parts Discussed in Thread: DRV2604, DRV2625,
Hello,
I can't seem to find too much information in the datasheet about running drv2604 in open-loop. Can you verify my understanding?
- In open-loop, the waveform sent to the LRA is PWM with a frequency determined by the DRIVE_TIME register. If my understanding is correct, it seems like there is an issue with the drv2604
- The frequency of vibration is different from the specified DRIVE_TIME value with our LRAs.
- Changes to DRIVE_TIME doesn't seem to affect the acceleration waveform.
With the drv2625 EVM, I was able to compare the PWM waveform played out to the LRA and the acceleration waveform and verify that the programmed frequency (via OL_LRA_PERIOD register) match.
There is no equivalent register as the OL_LRA_PERIOD for drv2604. Are you aware of any known issues with the open loop mode in the drv2604? Or do you know the proper way to program the drv2604 for open-loop operation at a specified frequency?
Thanks,
Nick