This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8353: confusion regarding the Evaluation board DRV8353

Part Number: DRV8353

Hello TI Team,

while searching about the BLDC motor driver, I came across the Evaluation board of DRV8353. 

is the program already embedded in to the evaluation board or should we program it?

which software should we use incase we have to program it. can i get some details of it?

also i want to know whether it can withstand our motor ratings not. please find the ratings of the motor below:

Motor 1: P rated - 3kW; I rated - 72A; I peak - 150A, Vin - 48V

Motor 2: P rated - 3kW; I rated - 50A; I peak - 150A-200A, Vin - 72V 

Motor 3: P rated - 10kW; I rated - 300A; I peak - 900A, Vin - 48V