Hi guys,
I have just bought a DRV8350H-EVM. I have successfully loaded the trapezoidal sensored FW, and motor is running correctly (although SLVUB78A says that it is needed to solder the unpopulated R82, R84, and R86 0 ohm, what I think is an errata because I do not find those resistors in the board, and in fact, my motor is running without doing that modification).
Now I want to design my own board, and I would like to get the design files of the EVM (mainly the schematic). I am not able to find them in the product site.
Thank you in advance.
Ramon Navarro