Other Parts Discussed in Thread: DRV8308
Hi,
i want spin my motor with closed loop. Speed range is 100 - 1400 rpm.
Start always with load at 100rpm.
The low starting speed is my problem.
The lowest start speed with closed loop i can realize is ~500rpm.
The Motor does not react if i choose a speed below 500rpm
My Motor: (4 Poles-Motor)
I use your TI development tool run the motor
this are the register-settings:
Speed change over a external CLK from function generator.
Is it possible to run such kind of motor at closed loop with 100rpm with the DRV8308 at all?
Can you check the Registers... maybe i missed something.
Best Regards
Michael M.