1. Which type of Transformer is used in the above circuit?
2. Inductor value ??
3. Which type of opto coupler is used?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
1. Which type of Transformer is used in the above circuit?
2. Inductor value ??
3. Which type of opto coupler is used?
he optocoupler input is full wave rectified AC and not DC. With increase in amplitude the current increases in optocoupler. As the triac fires at different phase, a PWM signal is generated accordingly at the output of optocoupler.
To learn more about the coupler used, please refer to www.ti.com/.../TIDA-00652 . The actual part used for the optocoupler is www.vishay.com/.../tsop311.pdf .
Hi.
Thanks for ur reply. actually i implement the circuit. bur every time r2 resistance burned. i used 2w resistance. may i know the reason for this issue