Other Parts Discussed in Thread: DRV8830, DRV8837
Hello,
I am using the DRV8832 in a minimal setup with ISENSE pulled low and VREF connected to VSET to disable current limit and drive the motor at maximum voltage. VCC is 5V decoupled with 2 x 0.1µF capacitors.
IN1 is pulled high and on IN2 applied is a PWM signal with 50% duty-cycle and 100Hz (red). The output voltage on OUT2 (yellow) looks like this (2V / 5ms):
Normally a 44.5 kHz output-signal would be expected but there is clearly something wrong.
Can anyone help me with this problem?
Regards
Daniel