Hi all
Would you mind if we ask DRV8814?
Our customer would like to DRV8814 for BDC at only A side Motor.
So, they don't use B side Motor.
Therefore we would like to confirm the termination of unused pins for B side.
We assume follow;
Bout1, 2 : OPEN
ENABLE/PHASE : Low(We assume that these pins have internal pull-down. Therefore, is it possible to be left floating?We could not find this information on the datasheet.)
BI0/1 : High or Low
BREF : 3.3V
BSENSE : GND
VMB : VMA with 0.1uF cap
If you have some advice, could you let us know?
Kind regards,
Hirotaka Matsumoto