Other Parts Discussed in Thread: DRV8814, DRV8841, DRV8842, DRV8843,
Hi,
I am using the DRB8813 in a non usual way, that is' I want to use the brake function of motor with four lower MOSFETs in ON state and upper MOSFETs in OFF state.
To achieve that, I've hard connect the AI0, AI1, BI0 and BI1 pins to 0 [Vdc] (selecting slow decay mode) and I switch the APHASE and BPHASE pins to rotate the motor: when I want brake rotation riducing power, I connect two pins AVREF and BVREF to 0 [Vdc], but the ouputs (AOUT1, AOUT2, BOUT1 and BOUT2) don't commutate to low voltage, because AOUT1 and AOUT2 continue to oscillate to 50 [KHz].
In all cases,if I drive APHASE = BPHASE = L.L.1 or APHASE = BPHASE = L.L.0, a single half of H bridge goes to low voltage and the other half oscillate to 50 [KHz].
How do I get the upper MOSFETs completely OFF and lower MOSFETs completely ON, without 50 [KHz] oscillation?
Thank you
Fabio